RealSense Support

New Depth Camera

Comments

1 comment

  • MartyX Grover

    Hi Mercio Jonova  Thanks very much for your questions.

     

    1.  1280x720 resolution is the depth resolution that will provide optimal accuracy on the D415 camera model.  Using the lower 848x480 should be fine too though if you find that you need to reduce the processing burden.  In regard to FPS, 30 should be fine, and in fact 1280x720 resolution does not support a higher FPS than 30. 

     

    If the robot will be fast-moving then using 848x480 and 60 FPS may provide better stability because the images will be updating more frequently.

     

    D415 is not best suited for fast-moving mobile applications (faster than a quick-waving human hand) because its depth and RGB sensors both use a slow Rolling shutter instead of the faster Global shutter.  Using 60 FPS will help to minimize lag / blur on the images when moving quickly or observing fast motion.

     

    2.  The RealSense depth sensing algorithm is robust against vibration, but there may be problems if the vibration is severe.  Introducing a vibration damping pad on the mounting point of the camera may help.

     

    If you use a USB cable with screw-locks on the end then you can firmly mount the micro-sized end of the cable to the side of the camera using screw-thread holes either side of the USB port on the camera to restrict the connector from moving within the port.

     

    The camera will be drawing power from the USB port on the robot, which in turn will be drawing power from the power supply unit of the robot's onboard computer.  So power stability to the camera will be dependent on the power delivery stability of the USB ports of the particular computer onboard the robot.

     

    3.  If an area has both light and shadow, a feature called High-Dynamic Range (HDR) can be used instead of auto-exposure to define an exposure range with two separate values.

    https://dev.realsenseai.com/docs/high-dynamic-range-with-stereoscopic-depth-cameras

    0
    Comment actions Permalink

Please sign in to leave a comment.