View my account

What's the best choice for a small movement track

Comments

1 comment

  • MartyX Grover

    Hi Sergiooooo17  If the small origami structure is not moving fast and depth / distance measuring accuracy is critical then the D415 model should be appropriate for your needs.  It has a minimum depth sensing distance of 0.3 meters / 300 mm and so should be able to depth-detect the origami if the camera will be positioned at least 500 mm from the structure.  The D415 also has around 2x less depth error over distance than the D435 / D435i models and has an optimal depth accuracy resolution of 1280x720 (compared to 848x480 on D435 / D435i and D455).

    https://store.intelrealsense.com/buy-intel-realsense-depth-camera-d415.html

    1
    Comment actions Permalink

Please sign in to leave a comment.