RealSense Support

Optimal way to shoot with a RealSense camera

Comments

3 comments

  • MartyX Grover

    Hi Dev Luenah  May I first confirm which RealSense camera model you are using, please.  The question is tagged as D400 Series but lidar is mentioned.  The 400 Series cameras are Stereo Depth technology, whilst the L515 model is Lidar.  Thanks!

    0
    Comment actions Permalink
  • Dev Luenah

    My using model is D435i.

    0
    Comment actions Permalink
  • MartyX Grover

    Thank you very much for confirming your camera model as a D435i stereo depth camera.

    Intel have a RealSense camera tuning guide at the link below that is a very good reference for advice on achieving improvement.

    https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance

     

    RealSense 400 Series cameras can make use of any visible light in a scene to analyze objects and surfaces in a scene for depth detail.  They can also obtain depth detail by projecting an infrared dot pattern onto surfaces in the scene.  The dot pattern is helpful for obtaining depth if a surface with low texture detail is being observed. 

    The dots would be cast onto the face and be readable as texture that is translatable into depth.  RealSense cameras are Class 1 laser devices that are safe for the face and eyes.

     

    Which type of lights are you using in your photography setup, please?  If they are fluorescent lights (like ceiling strip lights) then they could cause disruption to the camera image because they flicker at frequencies that are difficult to see with the human eye.  Use of LED photography lights would be preferable if you are not using them already.

    0
    Comment actions Permalink

Please sign in to leave a comment.