D457 Real Sense Camera USB port Connection
I have connected Real Sense D457 Camera to my PC through USB port, and try to detect the camera on Realsense Viewer, but not detected. Pleasse give solution for this.
-
Hi Amit Bohra By default the D457 is set to use a GMSL cable instead of USB. To set the camera to operate on a USB connection you need to open a small removable cover on top of the camera and move a physical switch beneath it sideways. Then the camera should be detected on USB as a D455 and have the same features and performance as a D455, with the added water and dust protection of the D457's IP65 casing.
The switch movement process is described at the link below.
https://support.realsenseai.com/hc/en-us/community/posts/14840675121043/comments/14843232242835
Please sign in to leave a comment.
Comments
1 comment