RealSense Support

D455 not detected by RealSense Viewer v2.56

Comments

4 comments

  • MartyX Grover

    Hi Patrycja Grabowska  Can you check the camera privacy settings in Windows please to ensure that permission for applications to access the camera is set to On.  Instructions for doing so can be found at the link below.

    https://github.com/IntelRealSense/librealsense/issues/3381#issuecomment-503424789

    0
    Comment actions Permalink
  • Patrycja Grabowska

    Hi MartyX Grover, thank you for your support. The solution has helped. However, I have new errors. Could you please assist?

    12:27:16 [None] C:\jenkins_sys_rsbuild\workspace\LRS_windows_compile_pipeline\common\notifications.cpp:539 - Frame Metadata is a device feature allowing
    software synchronization between different
    camera streams.
    It must be explicitly enabled on Windows OS

    12:27:17 [Error] C:\jenkins_sys_rsbuild\workspace\LRS_windows_compile_pipeline\tools\realsense-viewer\..\..\common\post-processing-worker-filter.h:51 - Cannot start Face Detection : OpenVINO: Error loading xmlfile: age-gender-recognition-retail-0013.xml, File was not found at line: 1 pos: 0

    0
    Comment actions Permalink
  • MartyX Grover

    Frame Metadata can be enabled on Windows in the RealSense Viewer tool.  When the program is launched, there will usually be a pop-up box that appears in the top corner informing that metadata is disabled and asking if you want to enable it.  You can then click a button on the pop-up to enable it.

     

    If you are experiencing the Face Detection error when launching the Viewer, you can download a standalone version of the Viewer that does not have the OpenVINO face detection feature and so will not trigger errors related to this feature.  To do so, please go to the link below and scroll to the Assets file list at the bottom of the page. 

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.56.5

     

     

    Left-click on the Intel.RealSense.Viewer.exe link to launch a download of this Viewer in your browser and then run the .exe file after download completes to launch it (do not launch the Viewer with a Windows desktop launch icon).

    0
    Comment actions Permalink
  • Patrycja Grabowska

    MartyX Grover, great, thank you for your help! 

    0
    Comment actions Permalink

Please sign in to leave a comment.