View my account

D455 Camera Stream FPS drops with Firmware 5.17.0.10

Comments

6 comments

  • MartyX Grover

    Hi Jingliang Tian  Which version of the RealSense SDK or RealSense Viewer are you using, please?  Firmware 5.17.0.10 is designed for use with SDK / Viewer version 2.56.5 or newer.

    0
    Comment actions Permalink
  • Jingliang Tian

    The SDK version is 2.55.1.6486 I used.    Thanks for your clarification.  Will try upgrade SDK version too.

    0
    Comment actions Permalink
  • Jingliang Tian

    Hi MartyX Grover,

    I have tested camera stream FPS in different scenarios.  Seems camera stream FPS be drops with camera firmware 5.17.0.10 and given dual USB hub chain no matter SDK versions.   Do you have any knowledge to share about this dual USB hub chain scenario?   Or I guess firmware 5.17.0.10 is not recommend base this hardware setup.

     

    Attach as details:

    Firmware: 5.17.0.10   SDK: 2.56.5.9235    Chain: dual USB hub chain (Camera → USB Hub → USB Hub → Host)      Camera stream lag

    Firmware: 5.17.0.10   SDK: 2.56.5.9235    Chain: Host directly USB (Camera -> Host)    Camera stream non-lag

    Firmware: 5.17.0.10   SDK: 2.55.1.6486     Chain: dual USB hub chain (Camera → USB Hub → USB Hub → Host)      Camera stream lag

    Firmware: 5.17.0.10   SDK: 2.55.1.6486    Chain: Host directly USB (Camera -> Host)    Camera stream non-lag

    Firmware: 5.15.1.55   SDK: 2.56.5.9235    Chain: dual USB hub chain (Camera → USB Hub → USB Hub → Host)      Camera stream non-lag

    Firmware: 5.15.1.55   SDK: 2.56.5.9235    Chain: Host directly USB (Camera -> Host)    Camera stream non-lag

    Firmware: 5.15.1.55   SDK: 2.55.1.6486    Chain: dual USB hub chain (Camera → USB Hub → USB Hub → Host)      Camera stream non-lag

    Firmware: 5.15.1.55   SDK: 2.55.1.6486    Chain: Host directly USB (Camera -> Host)    Camera stream non-lag

    0
    Comment actions Permalink
  • MartyX Grover

    The USB standard permits as many as five USB hubs to be linked together in a 'daisy chain'.  My research of the subject indicates though that devices spread across more than one hub may receive insufficient power or experience slowdown unless mains electricity powered hubs are used that are connected to the mains plug socket instead of drawing their power from the computer.  High power demand devices should all be attached to the first hub if possible.

     

    5.15.1.55 is classed as a Production firmware, meaning that it is recommended for use in critical-importance applications or commercial products that integrate RealSense because of Production firmwares' proven stability.  At the time of writing this, 5.15.1.55  is the most recent Production firmware.

    0
    Comment actions Permalink
  • MartyX Grover

    If you look at the firmware versions table, there is a field called Comment on the right-side that you may have to press the right-arrow key on your keyboard to scroll sideways to see properly.  Production firmwares have (P) at the top of their comments.

    https://dev.realsenseai.com/docs/firmware-releases-d400

     

    3
    Comment actions Permalink
  • Jingliang Tian

    Okay.  Got.  Will consider using 5.15.1.55. Thank you very much. Very helpful!

    0
    Comment actions Permalink

Please sign in to leave a comment.