RealSense Support

D555 is not recognized at all, out of the box

Comments

5 comments

  • MartyX Grover

    Hi Ryosuke Tajima  The link below has guidance from RealSense D555 users and from one of my RealSense colleagues with D555 expertise that may be helpful with your issue.

    https://github.com/IntelRealSense/librealsense/issues/14293

    0
    Comment actions Permalink
  • Ryosuke Tajima

    It seems very similar to my case, thank you! It may be a clue to me.

    0
    Comment actions Permalink
  • Ryosuke Tajima

    Thank you, the device worked properly! Even after reading the datasheet, I didn't realize that I could access the camera settings with just a USB cable, and I had mistakenly assumed that the configuration would be completed entirely through Ethernet. In reality, just like other RealSense devices, I simply needed to connect the USB cable first, check the settings (such as the IP address), and then connect via PoE - there were no problems at all.

    Thank you again.

    0
    Comment actions Permalink
  • Ryosuke Tajima

    By the way, regarding the LED mentioned in the original question, the result was that it doesn't light up at all, regardless of power supply or communication status. It may not be connected?

    0
    Comment actions Permalink
  • MartyX Grover

    It's great to hear that you achieved a working setup.  Thanks very much for the update!

     

    For information about the LED status, if you have a GitHub account then I recommend visiting the link above again and posting a comment about it, tagging the name @hsuys in the message to address it to my RealSense colleague.

    -1
    Comment actions Permalink

Please sign in to leave a comment.