View my account

Realsense D435 Products Containing Mercury Regulations (SOR/2014-254)

Comments

6 comments

  • MartyX Grover

    Hi YinBin Ng  All available regulatory certifications for RealSense cameras are available at the link below.

    https://realsenseai.com/regulatory-information/

     

    If a particular certification is not listed on this page then please assume that RealSense cameras have not been tested for it.

     

    SOR/2014-254 appears to be a Canadian regulation.  The data sheet document for RealSense 400 Series cameras provides the following regulatory information about the Canadian market on page 126 of the current edition.

    https://dev.realsenseai.com/docs/intel-realsense-d400-series-product-family-datasheet

    *************

    For the US and Canada market, this product has been tested and certified by UL and Nemko, and found to be compliant with all applicable requirements of the specifications below:


    UL 60950-1 2nd Edition, CAN/CSA C22.2 No. 60950-1-07, Information Technology Equipment – Safety Part 1: General Requirements

     

    Both UL and Nemko are Nationally Recognized Testing Laboratories (NRTLs), recognized by US Occupational Safety and Health Administration (OSHA) as qualified to perform safety testing and certifications covered within its scope of recognition.

     

    * Not applicable to D450, D401 modules and D455, D405 cameras 

     

    1
    Comment actions Permalink
  • MartyX Grover

    I located an Intel document from 2021 affirming the RealSense D455 camera's conformity with the European RoHS (Restriction of Hazardous Substances) regulation.  The RoHS restricted substance list includes mercury.

    https://www.intel.com/content/www/us/en/content-details/644828/intel-realsense-depth-camera-d455-eac-rohs-declaration-of-conformity.html

    0
    Comment actions Permalink
  • MartyX Grover

    Based on that link, I located the declaration of conformity with RoHS for the D435.

    https://www.intel.com/content/www/us/en/content-details/746827/camera-peripherals-intel-realsense-depth-camera-d435-declaration-of-conformity.html

    0
    Comment actions Permalink
  • YinBin Ng

    Hi MartyX Grover, thanks for all the helpful info.

    I located the MDDS for D435, and need some help on understanding the MDDS.

    If the declarable HM is stated "false" for "Above Threshold? (T/F)" column, and 0.00 or empty for "substance mass", does this means the HM is not used in the product?

    While HM with a stated "substance mass" means HM is used.

    0
    Comment actions Permalink
  • MartyX Grover

    A non-RealSense Intel document at the link below about the Above Threshold field in an MDDS document states that "Under the RoHS table, the False response to the Above Threshold (T/F) query indicates the substance is not present above threshold.  If a substance is above threshold, the response will be True and the substance mass percentage data and exemption information (if applicable) will also be provided".

    https://www.intel.com/content/www/us/en/support/articles/000059794/services/quality-regulatory-ecology.html

     

    The example MDDS table at the bottom of that document, where all of the Above Threshold fields are False and all of their Substance Mass fields empty, suggests to me - though I am not an expert on the subject of MDDS - that if the Threshold is False and Mass % of HM is empty then that element is indeed absent from the product.

    1
    Comment actions Permalink
  • YinBin Ng

    MartyX Grover Thank you for the clarification.

    0
    Comment actions Permalink

Please sign in to leave a comment.