View my account

Comments

1 comment

  • MartyX Grover

    Question: D435i authenticity verification.  How can we verify whether the D435i we bought through a third-party seller is genuine?

     

    Hello gao gao  Genuine RealSense cameras have a sticker on the base of the camera with a unique serial number.  If the serial number on the sticker matches the serial number displayed when using the 'Info' button in the RealSense Viewer tool's options side-panel or when using the command rs-enumerate-devices -s then your camera is likely to be genuine.

     

    If the tripod is attached to the base of the camera then you will have to unscrew and remove the tripod to read the sticker.

     

    你好@gao gao  正品 RealSense 相机底座上贴有标签,上面有唯一的序列号。如果标签上的序列号与使用 RealSense Viewer 工具选项侧面板中的“信息”按钮或使用命令 rs-enumerate-devices -s 时显示的序列号相符,那么您的相机很可能是正品。

     

    如果三脚架安装在相机底座上,那么您必须拧开并取下三脚架才能读取标签。

     

    0
    Comment actions Permalink

Please sign in to leave a comment.