RealSense Support

Real-time data storage using d455 depthcam.

Comments

1 comment

  • MartyX Grover

    If you are saving to .csv format then that is known to be slow, as mentioned by a RealSense team member in the link below.  Writing a bag format file is the most efficient RealSense recording method, though bag files can be gigabytes in size.  Bag files - which are like a video recording of camera data - can be recorded using pyrealsense2 scripting.

    https://github.com/IntelRealSense/librealsense/issues/1485#issuecomment-380728118

     

    It is possible though to save every frame as an individual bag file using an RealSense SDK instruction called save_single_frameset()

     

    Frames can also be stored in memory during recording with the Keep() instruction instead of continuously recording to file and then have batch-processing actions performed on all the frames when the recording is closed, such as alignment, post-processing and saving to file.  This method is suited to short recording durations though because it progressively consumes the computer's memory capacity.  On a Nano, 10 seconds would be a reasonable recording duration, whilst higher memory capacity computers could record to memory for 30 seconds.

    0
    Comment actions Permalink

Please sign in to leave a comment.