RealSense Support

IR Image with auto ir exposure is dimmer than manual on D415 cameras

Comments

6 comments

  • MartyG

    Hi Karthikeyan Yuvraj  I am reminded of a phenomenon demonstrated in the link below where the exposure and gain of the camera would drop to minimum level if auto-exposure was enabled and the camera was directly facing sunlight and therefore darken the infrared image. 

    https://github.com/IntelRealSense/librealsense/issues/4928

    In such circumstances, facing the camera away from the sunlight or holding a hand over the camera lenses for several seconds should result in auto-exposure correcting the image.

     

    Is your D415 in a location where it might be directly observing sunlight or a similar strong light source head-on, please?

    0
    Comment actions Permalink
  • Karthikeyan Yuvraj

    Hello MartyG,
    Thanks a lot for your reply. The camera is in an indoor location (and no sunlight), but the camera is facing straight ahead at the whiteboard (which is bright), maybe this is causing it?. Also, based on the thread you shared, can a firmware update fix this?.

    0
    Comment actions Permalink
  • MartyX Grover

    If the whiteboard had a reflective surface and light was being projected onto it then I can see how it could create a glare from the reflection that could have a negative impact on image quality.  

     

    There was a past case (in the link below) where a camera was located indoors in an office and tests with strong light projections such as an external flash and a laser pointer caused the camera to react as though it had faced the sun.

    https://github.com/IntelRealSense/librealsense/issues/5209#issuecomment-564483334

     

    Intel's camera tuning guide offers advice about dealing with strong light, such as defining an auto-exposure Region of Interest in the bottom half of the image.

    https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance#section-use-sunlight-but-avoid-glare

     

    The negative effects on the image of glare from reflections can also be greatly negated by purchasing and applying a physical thin-film linear polarization filter product over the lenses on the outside of the camera.  Intel's guide on optical filters provides information about this in section 4.4 When to use polarizers and waveplates

    https://dev.intelrealsense.com/docs/optical-filters-for-intel-realsense-depth-cameras-d400#section-4-the-use-of-optical-filters

    Any polarizer filter should work so long as it is linear (ones from 3D glasses will not work).  You can find examples by searching stores such as Amazon for the term linear polarization filter sheet

     

    Intel added a fix to the firmware as far back as firmware version 5.11.4 to correct the problem of the IR image going black when exposed to strong light whilst auto-exposure was enabled.  What firmware version is your camera using, please?

    0
    Comment actions Permalink
  • Karthikeyan Yuvraj

    thanks for the reply. My camera is at 05.11.01.100

    0
    Comment actions Permalink
  • Karthikeyan Yuvraj

    Ok fyi, I updated the camera to the latest version 05.13.00.50 and still, we have the same issue. 

    0
    Comment actions Permalink
  • MartyG

    Are you using RealSense SDK version 2.50.0

    0
    Comment actions Permalink

Please sign in to leave a comment.