RealSense Support

Extrinsic transform between the Depth stream and the Infrared stream

Comments

5 comments

  • MartyX Grover

    Hi Yixun Liu  Shown below is the rs-enumerate-devices -c listing of the 'Depth to Infrared 1' and 'Depth to Infrared 2' extrinsics from my own D435i, showing a different value on the 'x' translation coordinate of Infrared2.

     

     

    Could you try resetting the calibration of your camera to its factory-new defaults in the RealSense Viewer with the instructions in the link below and see whether it corrects your Infrared 2 translation x-value, please?

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink
  • Yixun Liu

    Thanks MartyG!

    I did as you said, from viewer->enable stereo module->more->calibration data->check I know what I'm doing->restore factory->write table, and then use the same command to list the extrinsic, but nothing change.

    0
    Comment actions Permalink
  • MartyX Grover

    I researched your issue further and found a case at the link below where the Infrared 2-Depth had the same extrinsics readout in rs-enumerate-devices as Infrared1-Depth.

    https://github.com/IntelRealSense/librealsense/issues/4050

     

     

    In the linked-to case, the RealSense user in that case also had the problem that any extrinsic that involved color, such as Color to Depth, had N/A beside it instead of listing the extrinsics like in the correct example from the image below.

     

     

    Do you have N/A beside your color extrinsics in your own rs-enumerate-devices listing, please?

    0
    Comment actions Permalink
  • Yixun Liu

    I do not have N/A issue and I list color to Infrared extrinsic as follows:

    Extrinsic from "Color"    To      "Infrared 1" :
     Rotation Matrix:
       0.999931        -0.0115592       -0.00189497
       0.0115613        0.999933         0.00108789
       0.00188227      -0.00110973       0.999998

     Translation Vector: -0.0148013643920422  -0.000198773050215095  -3.20835533784702e-05

    Extrinsic from "Color"    To      "Infrared 2" :
     Rotation Matrix:
       0.999931        -0.0115592       -0.00189497
       0.0115613        0.999933         0.00108789
       0.00188227      -0.00110973       0.999998

     Translation Vector: -0.0148013643920422  -0.000198773050215095  -3.20835533784702e-05

     

    I found my second D435i has different Color intrinsic from my first D435i. The values look different especially for principle point as shown in the following picture (in the image,the right side shows the copied values from the command output for the first D435i). As I know D435i use the same OminiVision OV9282 for the color image sensor. Why the values look different?

     

    My last question is if Intel continue its production for depth cameras such as D435i, D450 etc? 

    Thank you so much!

     

    0
    Comment actions Permalink
  • MartyX Grover

    Each camera has unique calibration values due to the manufacturing process in the factory (the cameras are calibrated in the factory), so it is normal for there to be differences between cameras.

    The 400 Series stereo depth camera range is continuing.  The L515 lidar depth model is not.

    0
    Comment actions Permalink

Please sign in to leave a comment.