RealSense Support

Error in RealSense Viewer

Comments

8 comments

  • MartyX Grover

    Hi Eriko Mogi  There have been a couple of past cases of this error, such as the one in the link below.

    https://github.com/IntelRealSense/librealsense/issues/1930

    If you are using Windows, please check in the Windows camera privacy settings that access to the camera hardware and permission for applications to access the camera are both set to On.  Instructions for doing so are here:

    https://github.com/IntelRealSense/librealsense/issues/3381#issuecomment-503424789

    0
    Comment actions Permalink
  • Eriko Mogi

    Thank you for your reply.

    I see the information.'Privacy Settings' option of camera was already On.

    librealsense's version is v.2.39.0. Should I upgrade realsense2.dll' version ?What is the difference between versions? 

    0
    Comment actions Permalink
  • MartyX Grover

    2.39.0 dates back to October 2020.  The SDK is now at 2.50.0 at the time of writing this and there have been a huge number of updates and bug fixes made to the SDK since 2.39.  So if you are able to upgrade your SDK version then I would strongly recommend trying that to see whether it resolves your problem.

    0
    Comment actions Permalink
  • Eriko Mogi

    I tried to apply realsense2.dll at 2.50.0. but an error has occurred.

    Backend in rs2_create_device(info_list:0A7EDB10, index:0):
    MFCreateDeviceSource(_device_attrs, &_source) returned: HResult 0x80040154: "クラスが登録されていません"

     

     

    0
    Comment actions Permalink
  • Eriko Mogi

    An error was detected in the following.

    1. Update the firmware of realsense, from v5.9.13.0 to v5.12.13.50.

    2.Upgrade OS version of PC connecting Realsense, windows10 1903 to 20H2.

    3.An error has occurred on Realsense Viewer.

    4.Update realsense2.dll v2.50.0. 

    Should I update dll file at first?

     

    0
    Comment actions Permalink
  • MartyX Grover

    It was a good idea to update your firmware from 5.9.13 to the recent version 5.12.13.50 first before using 2.50.0.  

     

    Can I confirm whether you are updating the entire RealSense SDK by downloading and running the Windows installer file in the 'Assets' file list on the SDK releases page and not just changing the realsense2.dll file?

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.50.0

     

    0
    Comment actions Permalink
  • Eriko Mogi

    Should I install the entire RealSense SDK to recognize Realsense on the Realsense Viewer ?

    I did not install SDK, install only realsense2.dll to operate an application developed.

     

    0
    Comment actions Permalink
  • MartyX Grover

    There are RealSense applications where you can simply substitute in an updated version of the RealSense DLL.  For the RealSense Viewer though, to use an updated version you should either update the entire SDK or instead download and run the small standalone pre-built version of the Viewer called Intel.RealSense.Viewer.exe from the 'Assets' file list of a particular SDK version on the 'Releases' page (see the image above).

     

    Intel.RealSense.Viewer.exe should be run with a double-leftclick from the folder location that it was downloaded to and not with the Viewer launch shortcut icon on the Windows desktop.

    0
    Comment actions Permalink

Please sign in to leave a comment.