L515 hot
1) One of our cameras become hot even if the computer is switched off but the camera power supply is ON. Is it OK that I have to switch off cameras?
2) what about best working temperature conditions for cameras?
-
Hi Golovin,
1) L515 camera requires a USB-C 3.1 cable to connect to host machine to provide power and transfer data during operation. Since, the supply power of the device is provided by the computer, hence when the computer is switched off, then the device should also switched off.
2) The ambient temperature range when the L515 camera is streaming should be in 0-30 °C.
Regards,
Yu-Chern
Intel Customer Support
Please sign in to leave a comment.
Comments
1 comment