RealSense Support

Hyperfocal distance of D435i RGB camera.

Comments

3 comments

  • MartyX Grover

    Hi Chandannaik999  I do not have an exact figure for hyperfocal distance (the distance below which the image can become blurred) when performing close range sensing.  On the D435 / D435i models though, a RealSense user was advised in the link below that whilst you may be able to move closer to an object than the D435i's minimum depth sensing distance of 0.1 meters (10 cm), the image may become blurred at 0.06 m (6 cm) or less because the imaging sensors of the D435 / D435i are not designed for such close range.

    https://github.com/IntelRealSense/librealsense/issues/7631

     

    If you only require the RGB image and not depth then you may be able to clear up blurring a little at very close range by using SDK options such as maximizing Sharpness, as discussed in this link:

    https://github.com/IntelRealSense/librealsense/issues/7187

    0
    Comment actions Permalink
  • Chandannaik999

    Thank you for your assistance. The images that I take are very close to the camera, less than 10cm. Would it possible to obtain a clear image for this particular case? (Note: I dont need the depth module)

    0
    Comment actions Permalink
  • MartyX Grover

    If you are only using RGB then distance from the object should not be so much of an issue.  To demonstrate this I used a D435i to capture keyboard keys at 1, 2 and 3 cm height from the keyboard respectively to highlight the blurring that might be expected at extreme close range.

    These are unaltered images with no sharpening applied to them.

     

    1 CM

     

    2 CM

     

    3 CM

    0
    Comment actions Permalink

Please sign in to leave a comment.