View my account

Drive for Intel(R) RealSense(TM) Camera SR300 Virtual Device?

Comments

3 comments

  • MartyX Grover

    Hi Pedro Gomezgarcia  In the Dispostivos de imagen section of the Device Manager, please right-click on the SR300 Depth driver and select the Uninstall option.  Unplug the SR300 camera and wait a couple of seconds and then plug the camera back into the USB port.  The drivers should then automatically reinstall.

    0
    Comment actions Permalink
  • Pedro Gomezgarcia

    Hi MartyG, I'm using a laptop and my camera is a built-in, how can I "Unplug" the device?

    0
    Comment actions Permalink
  • MartyG

    RealSense cameras that are built into a computer are significantly more difficult than the USB models to repair if they have a problem, unfortunately.  In this particular case it is likely the absence of the removed software driver that is causing the problem rather than a hardware fault though, which does slightly increase the chances of achieving a solution.

    The first step I would recommend is to find whether the manufacturer of your laptop has a technical support website, and if it does then can the camera drivers for your model of laptop be downloaded from that site. 

    0
    Comment actions Permalink

Please sign in to leave a comment.