RealSense Support

D435 Cameras - Lighting conditions

Comments

1 comment

  • MartyX Grover

    Hi Gbi  The RealSense 400 Series cameras can make use of ambient light in a scene to analyze surfaces for depth detail.  In a dimly lit scene though, enabling the camera's IR Emitter component to project a semi-random dot pattern onto the objects in the scene enables the camera to use those dots that are cast onto surfaces as an analyzable texture source instead.

    In a dark scene, external light sources such as an IR illuminator lamp can also be used to provide the camera with light that it can make use of.

    A chart in the link below provides suggestions for minimum exposure-time values to use at particular lux levels for best depth performance.

    https://dev.intelrealsense.com/docs/high-speed-capture-mode-of-intel-realsense-depth-camera-d435#section-4-1-minimum-required-exposure-time

    0
    Comment actions Permalink

Please sign in to leave a comment.