RealSense Support

Connect D455 to Jetson Xavier NX through MIPI-CSI

Comments

1 comment

  • Aznie Syaarriehaah

    Hi Joseslava,

    The D400 series cameras can be used with a wide variety of host platforms, as long as they can have robust USB 3 ports and run Ubuntu or Windows. Some low-power boards have difficulty delivering the required power via their USB subsystems. The RealSense cameras are not validated with NVidia boards so support for these boards is provided mainly by the NVidia community.

    Meanwhile, MIPI is not currently supported. 

    Regards,
    Aznie

    Intel RealSense Customer Support 

    0
    Comment actions Permalink

Please sign in to leave a comment.