Part Number (with USB type C cable)
What is the ordering part number for the part numbers mentioned below that come together with USB type C cable? I believe that the part numbers in below are without the cable.
1) PN#82635ASRCDVKHV
2) PN#82635ASRCDVKMP
Please advise.
Thanks.
-
Hi Kent Liew
If you are enquiring where you can obtain USB Type-C cables for RealSense 400 Series cameras, a company called Newnex can supply high quality USB cables that are validated for use with RealSense cameras.
https://www.newnex.com/realsense-3d-camera-connectivity.php
https://www.youtube.com/watch?v=GLQgR1jT04M
-
Newnex have been previously quoted in the official RealSense technical data sheet document as a logistics source for USB cables for 400 Series cameras, so I would recommend querying to them about cable supply.

Individually boxed units of 400 Series cameras are supplied with a USB Type-C cable and tripod. So if you purchased a quantity of 30 individually boxed units, for example, then they would come with the cable.
https://store.intelrealsense.com/
RealSense 400 Series cameras are out of stock in the official RealSense Store and most major RealSense stockists at the time of writing this. The company Rutronik24 apparently still have stock of 400 Series cameras though, including the D415.
https://www.rutronik24.com/search-result/qs:realsense/reset:0
-
I would add of course that USB Type-C cables that will fit the camera can be obtained from other suppliers / manufacturers. The most important factor is that the cable is high quality, especially when using cable lengths of 2 meters or more (the official cable supplied with the individually boxed cameras is 1 meter). If your customer prefers to order from a local supplier, it may be best for them to order one cable from that supplier first to test it with their cameras to validate that it works well with RealSense before placing a bulk order of that cable.
Please sign in to leave a comment.
Comments
4 comments