RealSense Support

L515 sometimes displays consistent offset in depth values

Comments

1 comment

  • Zulkifli Halim

    Hello Pharvey,

     

    We apologize for the delay in response.

     

    The depth error average at 1m distance from the camera is <5mm. The reflexibility for the target to reflect the infrared back to the camera might be the issue. 

     

    The current workaround that you can use is to change the preset to adjust the laser power and the receiver gain. We are still looking for the right method to encounter this issue. 

     

    Sincerely,

    Zulkifli

     

    0
    Comment actions Permalink

Please sign in to leave a comment.