View my account

Does L515 able to get depth of objects which are under water

Comments

1 comment

  • Munesh

    Hi Qing1 Zhang,
    Thanks for reaching out to us.

    The performance from depth sensing underwater can vary due to the possible different lighting conditions, as well as conditions under the water's surface. I would suggest you have a look at the following project to get an idea about the depth sensing quality underwater:

    FishSense
    A project between Engineers for Exploration (E4E) students with collaborators from Scripps Institute of Oceanography. Their webpage mentions that they are using D455 camera. The introductory video also mentions using D435 and L515 cameras for their project.
    Watch their two videos below:

     

    Additionally, please refer to the following paper as well:

    Underwater 3D capture using a low-cost commercial depth camera


    Regards,
    Munesh
    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.