View my account

Need RealSense 2016 R3 SDK + Runtime Essentials

Comments

3 comments

  • MartyX Grover

    Hi Jay The Intel downloads hub-page for the 2016 SDK is no longer available.

    You can though download the 2016 Windows SDK's 'R2' version from the direct link below.  Clicking on the link will launch a 1.8 GB download of the installer file for the SDK in your browser.  The main difference between the R2 and R3 SDKs is that R2 installs the entire SDK, whilst R3 took the approach of dividing the SDK's features up into multiple optional modules.  So I would highly recommend using 2016 R2 for its everything-included ease of use.

    http://registrationcenter-download.intel.com/akdlm/irc_nas/vcp/9078/intel_rs_sdk_offline_package_10.0.26.0396.exe

     

    If the above link does not launch when left-clicked on, you can copy and paste the address into your browser address window and that should work too.

     

    The official PDF programming manuals for the 2016 SDK can be downloaded as a zip-file attached to the bottom of the comment at the link below.

    https://community.intel.com/t5/Items-with-no-label/RealSense-2014-SDK-manuals-and-script-samples/td-p/482383?profile.language=en

    0
    Comment actions Permalink
  • MartyG

    I should emphasize of course that downloading .exe files from the internet is generally a bad idea because of the risk of viruses, malware, etc.  This is an official link directly to an Intel download server in this particular case though.

    0
    Comment actions Permalink
  • Jay

    MartyG,

     

    Many thanks for posting the above link to the RealSense 2016 R2 SDK off-line installer. 

    We will give it a go and see if we can get it working ....

    Cheers

    Jay

    0
    Comment actions Permalink

Please sign in to leave a comment.