RealSense Support

Can I assemble a better than the D455?

Comments

4 comments

  • MartyG

    Hi Mau  If your intention is to capture data from two cameras and combine their individual viewpoints from different locations and perspectives into a single one then that can certainly be achieved.  For example, if you generate a point cloud from each camera then the two clouds can be 'stitched' together and an affine transform process then be applied to position and rotate the clouds into a common 3D space.  In this way, a 360 degree scan can be produced.

    The RealSense volumetric capture article linked to below provides an excellent introduction to the concept of merging multiple cameras into a combined final image.

    https://www.intelrealsense.com/intel-realsense-volumetric-capture/

    0
    Comment actions Permalink
  • Mau

    Thank you for the prompt response Marty!

    Also thank you for the article, it is definitely useful.

    I am also interested on increasing the distance between depth sensors to more than 95mm.

    Do you know if it is viable to use two D455 to work as one stereo camera with an increased depth accuracy?

    I was thinking of mounting them 1 meter apart at least.

    0
    Comment actions Permalink
  • MartyG

    The baseline distance of RealSense cameras is fixed.  You can though place two or more cameras in a horizontal row or a vertical stack and combine their individual overlapping fields of view (FOV) into a single larger one. 

    This may provide an improved depth image by increasing the density of analyzable dots cast into a particular area by the projectors of the cameras and also incorporate redundancy into the depth data by having more than one camera observe the same area where the FOVs overlap. 

     

    Furthermore, the more cameras you use then the fewer blind-spots there are in the observed scene.  For example, you may be able to create 360 degree coverage of a scene with a circle of six inward-facing cameras, but more would be better.

     

    You can also add physical optical filter products over the lenses on the outside of the camera to further customize  the camera to your project's particular needs.  Intel have published a white-paper document on this subject.

    https://dev.intelrealsense.com/docs/optical-filters-for-intel-realsense-depth-cameras-d400

     

    There are ways in which the depth map can be enhanced through software settings too.  An example of this is Intel's white-paper about improving depth on drones.

    https://dev.intelrealsense.com/docs/depth-map-improvements-for-stereo-based-depth-cameras-on-drones

    0
    Comment actions Permalink
  • MartyG

    I tried posting some further resource links but they would not appear on the forum.  You can find them instead by googling the following terms.

     

    realsense webinars

    realsense white papers

    realsense youtube channel

    0
    Comment actions Permalink

Please sign in to leave a comment.