RealSense Support

Comments

10 comments

  • Yu-Chern Peh

    Hi Rahul R,

     

    If you connect your F455 to an Android device before, please refer to this post.

     

     

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Rahul R

    I didn't connect with Android device, i had connected with raspberry pi and it's suddenly not working and it's giving this error, please give me solution asap.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Rahul R,

     

    Try to build with secure communication enabled by following this instruction. After that, unpair it for the use of non-secure mode. 

    Run the command: rsid-cli.exe <port> and insert 'i' to unpair with the device (disables secure communication).

     

     

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Rahul R

    I m getting this error now, earlier it was working fine. i m quite confuesd can you give me clear solution for this dear. 

    Thanks .

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Rahul R,

     

    Was your issue solved previously by updating the firmware? Are you using the different versions in Windows and Raspberry Pi? 

     

    I would suggest you do a fresh installation again. Connect the F455 to Windows, and uninstall first. Then, re-install the latest version, rsid_sdk_v0.21.0_signed_win64.exe.

    Download this firmware, F450_3.1.0.29_SKU1_SIGNED.bin and upload the firmware by running rsid-fw-update.exe with the command:

    rsid-fw-update.exe --file "<downloaded_dir>\F450_3.1.0.29_SKU1_SIGNED.bin" --port <COM?> --force-version

    After the firmware is updated successfully, download this firmware, F450_4.0.0.37_SKU1_SIGNED.bin and upload it again.

    rsid-fw-update.exe --file "<downloaded_dir>\F450_4.0.0.37_SKU1_SIGNED.bin" --port <COM?>


    Right-click Intel RealSense ID Viewer in the Desktop and then select "open file location".
    The rsid-fw-update.exe file is located there.

    Try running the Intel RealSense ID Viewer. If everything works fine in Windows, re-compile again in Raspberry Pi. Remove all the folders in Raspberry Pi. 

     

    git clone -b v.21.0 https://github.com/IntelRealSense/RealSenseID.git
    cd RealSenseID
    mkdir build
    cd build
    cmake ..

     

    Hope this helps.

     


    Regards,
    Yu-Chern
    Intel Customer Support

     

    0
    Comment actions Permalink
  • Rahul R

    Thanks a lot , It's working fine. 

    But still i m having doubt. when i insert p then it's showing pairing start and stop . but when i insert I it's showing start and ok no stop is there.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Rahul R,

    If I am understanding you correctly, you compile with the option -DRSID_SECURE=1 during the CMake in Raspberry Pi. Then, Raspberry Pi is already paired with the device. So, it won't take effect after you insert 'p'. Can you try with insert 'i' to unpair and then insert again 'p'? 

     

    Please note that you have to insert 'i' to unpair the device with the Raspberry Pi before you connect the device to another host machine. 

     

     

    Regards,
    Yu-Chern
    Intel Customer Support

    0
    Comment actions Permalink
  • Rahul R

    ok Thanks it's working fine now. Yu-Chern Peh

    0
    Comment actions Permalink
  • Rahul R

    When updating version 4.2 than it is showing this error and if i m giving 3.1 version file it is showing for 4.2 and above. and i download new 4.2 sdk also .

     

    0
    Comment actions Permalink
  • Rahul R

    Thanks,

    The problem has been solved. 

    0
    Comment actions Permalink

Please sign in to leave a comment.