View my account

Realsense camera connection fails at first try in every day.

Comments

1 comment

  • MartyX Grover

    Hi Sungbae9023  as a starting point in investigating your case, may I ask you the following questions please.

    1.  Which version of the RealSense SDK (librealsense) are you using?

    2.  Are your two USB 3 hubs mains electricity powered or are they 'passive' hubs that draw their power from the computer / computing device that they are attached to?

    3.  Do the hubs have 4 or more ports?  If so, is it possible to attach all 4 cameras to the same hub?  This would ensure that all of the cameras were handled by a USB controller from the same manufacturer.

    If you are unable to have all cameras on the same hub due to bandwidth limits then two hubs of the same model from the same company may address the issue of keeping the manufacturer of the USB controller consistent between ports.

    0
    Comment actions Permalink

Please sign in to leave a comment.