View my account

Depth map of a flat surface with D415

Comments

1 comment

  • MartyX Grover

    Hi Miguel Ares  If the surface that the camera is observing is flat and has low texture or no texture (like the white wall that your camera is pointed at) then turning off the IR emitter may indeed not be a suitable course of action.  This is because the projection of dots onto a surface provides texture for the camera to analyze for depth information.  400 Series cameras can alternatively use ambient light in a well-lit scene to obtain depth information in the absence of a dot pattern, but this may not be practical for a textureless surface.

     

    You could consider using an external LED pattern projector to project a dot pattern instead of the built-in laser projector of the camera.  The camera's laser-based projector can cause a noise effect on the image called laser speckle.  A dot pattern cast by an LED projector will produce significantly less speckle.  Intel have a white-paper document about use of projectors with 400 Series cameras at the link below.

    https://dev.intelrealsense.com/docs/projectors

    0
    Comment actions Permalink

Please sign in to leave a comment.