F455: IP code, moisture condition requirement
Hello,
Could you tell me the following information of F455 peripheral?
If Intel doesn't have those specs officially, then please reply so.
-IP code: Ingress Protection Code is defined in IEC standard 60529.
example: IP40.
FYI: https://en.wikipedia.org/wiki/IP_Code
-Moisture spec: moisture condition that is required at the operation.
example:20-80% non condensing
Note:
I tried to find those in the product datasheet, product web page, and the regulatory declarations sheet.
Also, I searched the knowledgebase and community article using the keyword such as "F455 water", "F455 IP code" and "F455 moisture". But it was not successful.
Thank you,
Kunio Horie
Please sign in to leave a comment.
Comments
2 comments