RealSense Support

camera d435 detection error

Comments

3 comments

  • MartyG

    Hi Luciano Fernandez. I believe that most of the log is just a record of the program's normal operations and the only significant line of the log is the final one.

    RuntimeError: set_xu(id=2) failed! Last Error: Input/output error

     

    This error indicates some kind of temporary communication problem with the camera has occurred that can be corrected with a camera reset or a USB unpug-replug.  If the camera is plugged into a USB 3 port, possibly the camera has been mis-identified as being on a USB 2 connection instead of USB 3 during one of the launches of the program.

    -1
    Comment actions Permalink
  • Luciano Fernandez

    I have been able to fix this, updating the camera firmware. This problem is related to this issue:

    https://github.com/IntelRealSense/librealsense/issues/2932

    0
    Comment actions Permalink
  • MartyG

    Great to hear that you found a solution that worked for you, Luciano Fernandez - thanks for the update!

    0
    Comment actions Permalink

Please sign in to leave a comment.