[D457] Ma96712 + intel d457 in the Nvidia jetson platform
Hi
I have an ODM project where the deserializer is a Max96712 connected to an Intel D457.
I only see the source code for max9296 + max9295 in the master branch.
May I ask if there is source code for JetPack 6.2 with max96712 + max9295?
https://github.com/IntelRealSense/realsense_mipi_platform_driver
-
Hi Kevin Liao Thanks very much for your question. I see that you have also posted the question on the RealSense MIPI driver support forum. That is the correct place to receive advice about using the D457 in GMSL mode.
https://github.com/IntelRealSense/realsense_mipi_platform_driver/issues/289
Please sign in to leave a comment.
Comments
1 comment