RealSense Support

Gimbal Recommendation for Intel RealSense D435i camera

Comments

1 comment

  • MartyX Grover

    Hi Reshteen Khostval  In the downloadable PDF user guide for the Dynamic Calibration tool, there is a section at the end of the guide that has a tutorial guide for using a WidowX MX28 Robot Turret gimbal by Trossen Robotics.  This is the only RealSense-validated gimbal product that I am aware of.

    https://dev.realsenseai.com/docs/intel-realsensetm-d400-series-calibration-tools-user-guide

     

     

    If the D435i camera will be attached to the gimbal via the two small mounting holes on the rear of the camera (like in the above image) then you may be able to find a gimbal that fits it so long as the gimbal has M3 size mounting screws to fit the standardized M3 size mounting holes on the rear of the D435i.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.