RealSense Support

Unable to Detect D457 Camera on Windows 11

Comments

1 comment

  • MartyX Grover

    Hi Xuanye Zeng  The D457 camera model is set by default to be used with a different type of cable called GMSL.  In order for the camera to be detected when used with a USB cable, you need to remove a small cap on the top of the camera casing and move a physical switch sidewards into the 'USB' position.  The camera should then be detected.

     

    If it is still not detected, unplug the micro-sized end of the USB cable from the base of the camera, turn the connector around the other way and re-insert it into the camera.

     

      More information about configuring the physical switch can be found here:

    https://support.realsenseai.com/hc/en-us/community/posts/14840675121043/comments/14843232242835

    0
    Comment actions Permalink

Please sign in to leave a comment.