View my account

Inter camera synchronization using an arduino

Comments

1 comment

  • MartyG

    Hi Mauriello  When performing hardware sync with an external trigger signal, it can be difficult as the generated signal has to have a frequency that is matched very closely with the FPS of the camera, which may not be 30 exactly.  Please try a trigger frequency of 30.015

     

    It is much easier to sync an external trigger if the genlock type of hardware sync is used.  With this, you would set the camera to 30 FPS and its Inter Cam Sync Mode to 4 instead of 2, and set the trigger frequency to half of the camera FPS - so if the camera FPS is 30, set the trigger frequency to 15 Hz.

    0
    Comment actions Permalink

Please sign in to leave a comment.