Intel Real sense D435 with Unity
I'm working on a real-time tracking project that integrates motion data with 3D content in Unity. I'm using the Intel RealSense D435 camera for motion tracking, and I understand that I need the Unity wrapper to get it working. However, I'm running into issues — the wrapper isn't functioning properly in Unity and keeps throwing errors. I would really appreciate any help you can provide to resolve this problem.
-
Hi Halabyehayat The RealSense Unity wrapper is no longer updated, and the last update it received was several years ago in RealSense SDK version 2.47.0 in June 2021. So it will not have been tested with Unity versions from recent years either. I have used it with the Unity 2021 version though.
Are you using Windows, please? And if you are, what is the RealSense SDK (librealsense) version you are using?
If the motion you are tracking is a human body then if it is possible for you to use pre-made commercial software then I would recommend the D435-compatible body tracking tool Nuitrack SDK, which has Unity integration.
Please sign in to leave a comment.
Comments
1 comment