Technical Support Request - Q121532
Hello,
Could you please help me to advise to Customer what part number he needs to order for below:
DEPTH CAMERA D457- DEPTH SENSOR
+ RGNB
+ FAKRA GMSL2 CONNECTRO,
+ HARDWARE PTP SYNCHRONIZATION.
Is the part number: 82635DSD457 correct one?
Thank you for assistance,
-
Hi Grzegorz Bartosz Yes the part number 82635DSD457 is the Product Code for a single D457 camera. If they want a multi-pack of the camera then MP is added onto the end of the code.

-
In the D457 camera product, almost everything needed to set it up on a FAKRA GMSL cable connection, including the FAKRA GMSL connector and hardware sync pins, is built into the camera.
It will be necessary though to separately purchase a deserializer module in order to receive data from the camera on a GMSL FAKRA cable connection. Information about D457-compatible deserializers can be found here:
https://github.com/IntelRealSense/librealsense/issues/10984#issuecomment-2413323360
Alternatively, if the D457-cmpatible computing system by Connect Tech is purchased then it is not necessary to purchase a deserializer as the technology is built into their system.
Ideally, the D457 should be used with a Jetson Xavier or Jetson Orin computing board.
It is also necessary to install a RealSense MIPI driver software to use the camera with the RealSense SDK software. If the customer does not use a Jetson Xavier or Orin as their computer then they will need to convert ("port") the driver themselves for use with their choice of computing hardware.
https://github.com/IntelRealSense/realsense_mipi_platform_driver
Please sign in to leave a comment.
Comments
3 comments