View my account

Technical Support Request - Q121532

Comments

3 comments

  • MartyG

    Hi Grzegorz Bartosz  Yes the part number 82635DSD457 is the Product Code for a single D457 camera.  If they want a multi-pack of the camera then MP is added onto the end of the code.

     

     

     

     

    0
    Comment actions Permalink
  • Grzegorz Bartosz

    Hello,

    Could you advise what about the below hardware:

    + RGNB

    + FAKRA GMSL2 CONNECTRO,

    + HARDWARE PTP SYNCHRONIZATION.

    Is this included into that part?

    Thanks

    0
    Comment actions Permalink
  • MartyG

    In the D457 camera product, almost everything needed to set it up on a FAKRA GMSL cable connection, including the FAKRA GMSL connector and hardware sync pins, is built into the camera.

     

    It will be necessary though to separately purchase a deserializer module in order to receive data from the camera on a GMSL FAKRA cable connection.  Information about D457-compatible deserializers can be found here:

    https://github.com/IntelRealSense/librealsense/issues/10984#issuecomment-2413323360

     

    Alternatively, if the D457-cmpatible computing system by Connect Tech is purchased then it is not necessary to purchase a deserializer as the technology is built into their system.

    https://connecttech.com/connect-tech-offers-built-in-support-on-the-newly-announced-intel-gmsl-realsense-depth-camera-d457/

     

      Ideally, the D457 should be used with a Jetson Xavier or Jetson Orin computing board.

     

    It is also necessary to install a RealSense MIPI driver software to use the camera with the RealSense SDK software.  If the customer does not use a Jetson Xavier or Orin as their computer then they will need to convert ("port") the driver themselves for use with their choice of computing hardware.

    https://github.com/IntelRealSense/realsense_mipi_platform_driver

    0
    Comment actions Permalink

Please sign in to leave a comment.