RealSense Support

ROS Humble Cloud Point Problem D435i (Jetson Nano Orin)

Comments

4 comments

  • Eliezerjustin4

    Another thing that I would like to add is when first launching the camera through ros2, from ros2 topics list, pointcloud does not show. After searching online I found this code that enables it: ros2 launch realsense2_camera rs_launch.py align_depth:=true pointcloud.enable:=true. I do not know if this adds any helpful information, but I hope that this information can help anyone to better understand the problem.

    0
    Comment actions Permalink
  • MartyG

    Hi Eliezerjustin4  When generating a pointcloud in ROS2, unless you need the aligned-image topics then you do not need to include the align_depth.enable:=true parameter in your launch as depth and color will be mapped together automatically when pointcloud.enable:=true is used.

     

    The warning No stream match for pointcloud chosen texture Process - Color indicates that RGB color frames are being dropped during streaming.  What happens if you use the launch command below to disable the color image and also disable texturing of the pointcloud?

     

    ros2 launch realsense2_camera rs_launch.py enable_color:=false pointcloud.enable:=true pointcloud.stream_filter:=0

     

    0
    Comment actions Permalink
  • Eliezerjustin4

    Hi MartyG,

    Thank you for your response. RVIZ started giving me this error:


    [INFO] [1742144592.857645602] [rviz]: Message Filter dropping message: frame 'camera_depth_optical_frame' at time 1742144591.356 for reason 'discarding message because the queue is full'
    Also is there a way to fix the frame dropping of the camera that is indicated by:
    [realsense2_camera_node-1]  12/03 23:05:17,591 WARNING [281472921168096] (messenger-libusb.cpp:42) control_transfer returned error, index: 768, error: Resource temporarily unavailable, number: 11

     

    0
    Comment actions Permalink
  • MartyG

     

    0
    Comment actions Permalink

Please sign in to leave a comment.