RealSense Support

D435 with Labview 32 bit

Comments

1 comment

  • MartyG

    Hi B Bala3703  If you are using RealSense SDK version 2.33.1 with the RealSense LabVIEW wrapper then I recommend using the newer SDK version 2.51.1 with it instead.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.51.1

     

    You can install 2.51.1 by visiting the above link and scrolling down the page to the 'Assets' file list, then downloading and running the Intel.RealSense.SDK-WIN10 automated installer program file.

     

     

    After installation, you can go to the location below on your Windows computer to obtain the 32-bit (x86) version of the realsense2.dll file for SDK 2.51.1.

    C: > Program Files (x86) > Intel RealSense SDK 2.0 > bin

     

    Then use this DLL file from SDK 2.51.1 with the LabVIEW wrapper instead of 2.33.1.

    0
    Comment actions Permalink

Please sign in to leave a comment.