RealSense Support

"Using Pre-Recorded Data for Box Measurement and Multi-Camera Calibration in Python"

Comments

5 comments

  • MartyG

    Hi Araj7322  You can use a pre-recorded bag file as the data source in a script instead of a live camera simply by inserting an enable_device_from_file() config instruction directly before the pipeline start line of the script.  This principle is demonstrated in the RealSense SDK's Python example script read_bag_example.py

    https://github.com/IntelRealSense/librealsense/blob/master/wrappers/python/examples/read_bag_example.py#L42

    0
    Comment actions Permalink
  • Araj7322

    Thank you, MartyG. Can we calculate the 3D dimensions of an object using the Box Dimensioner Multi-Cam code in Python with a pre-recorded .bag file? If so, how can we implement that? Also, since only limited .bag pre-recorded files are available, are there any additional .bag files available that can be used for this task?

    0
    Comment actions Permalink
  • MartyG

    I cannot recall a previous case where bag files have been used instead of a live camera with the box_dimensioner_multicam project.  It may still work though if you try adding a bag import instruction to the project's code.

     

    Some official sample bag files for testing can be found at the link below.

    https://github.com/IntelRealSense/librealsense/blob/master/doc/sample-data.md

     

    I would expect though that those bags would not be useful for use with box_dimensioner_multicam though as they are not focused on a box object.

    0
    Comment actions Permalink
  • Araj7322

    Thank you MartyG for your response.

    0
    Comment actions Permalink
  • Neighsanlo

    This is useful for me.

    0
    Comment actions Permalink

Please sign in to leave a comment.