RealSense Support

help me fix SR300 drivers

Comments

3 comments

  • MartyG

    Hi Emersongcardona  I see that your Device Manager has the three required SR300 drivers (Depth, RGB, Virtual).

     

    However, the SR300 camera model was retired a long time ago.  If you are trying to use the camera with the RealSense SDK or the RealSense Viewer tool, you will need to install version 2.50.0 of them as that was the final version to support SR300.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.50.0

    1
    Comment actions Permalink
  • Emersongcardona

    hello MartyX Grover thanks that works, but i am not sure if the camera is working properly, could you tell me witch is the later intel realsense depth camera manager that is compatible with the SR300 to install the drivers? i use to use the  intel_rs_dcm_sr300_3.4.104.3435 but doesnt work anymore in this computer (in windows 10 i only ran this driver and camera used to worked fine)

    0
    Comment actions Permalink
  • MartyG

    Since 2017 you do not need the DCM program to install the SR300 drivers on Windows.  If they are not present then they are installed automatically when the camera is inserted into the USB port if you have an active internet connection.

    0
    Comment actions Permalink

Please sign in to leave a comment.