View my account

L515 external hardware sync information

Comments

2 comments

  • Zulkifli Halim

    Hello T Loomans,

    Thank you for contacting us.

    1. 3.3V is the only validated voltage value for the sync signal. Do not use any voltage other than 3.3V.
    2. Section 1. Connecting the cameras of the L515 Multi-Camera paper shows that no extra resistors are necessary.
    3. Section E. External Trigger shows the timing diagram. Frame capture begins immediately after the 60 ms setup time and this cannot be changed.
    4. A full 33 ms is required to capture a frame. This corresponds to the fixed 30 fps framerate -- 1 second/30 fps = 33 ms. The frame rate is fixed at 30 fps so the 33 ms cannot be changed.

    Regards,

    Zulkifli

    0
    Comment actions Permalink
  • T Loomans

    Dear Zulkifli,

    Thank you for the response. After some experimentation and another support question I've found out that your answer is actually incorrect. According to the answer from Jesus, the setup time is not exactly 60.000ms but it can differ between triggering.

     

    So setup time is about 2 frames (60ms ~= 2*33ms) before a good frame is available.

    It will depend on where in the cycle the sync signal is high. You may go high with the sync signal when a frame is already in the middle of its presentation.

     

    Also the frame capture doesn't start immediately after 60ms, the camera is always capturing and frame transfer only happens when the external trigger is high for a complete capture cycle after the setup time.

     

    With kind regards.

    0
    Comment actions Permalink

Please sign in to leave a comment.