RealSense Support

Getting segmentation faults with Intel Realsense Cameras

Comments

5 comments

  • MartyG

    Hi Kevin Chow  The segmentation faults in the RealSense Viewer that you are experiencing are likely not related to how recent the SDK version is.

    Do you have segmentation faults when only one camera is attached to the computer, please?

    0
    Comment actions Permalink
  • Kevin Chow

    Hi MartyG, I get them with both 1 camera is attached or 2. It happens when I simply turn on a stream (depth or colour) and then turn said stream off via the realsense-viewer.

    0
    Comment actions Permalink
  • Kevin Chow

    My current system conditions are:

    OS: Ubuntu 18.04.5

    Cameras: D415 with firmware version 5.12.10.00

    Realsense-viewer: v2.41.0

    My most common situations for seg faults arising is:

    (1) When I go to view my second camera and select it, the entire realsense-viewer freezes and then segmentation faults.

    (2) When I turn on the depth stream and then the colour stream and then move to turn 1 of those streams of (any)

    0
    Comment actions Permalink
  • Kevin Chow

    The most reliable way to trigger this segmentation fault is with 2 cameras, if you turn on all camera streams and then turn off any of the streams. The realsense-viewer freezes up and then crashes with a segmentation fault.

    0
    Comment actions Permalink
  • MartyX Grover

    I will continue this case at the GitHub version that you posted so that we are not communicating in two places at the same time.  Thanks!

    https://github.com/IntelRealSense/librealsense/issues/8154 

    0
    Comment actions Permalink

Please sign in to leave a comment.