View my account

Build Dependencies for Unity integration

Comments

4 comments

  • MartyX Grover

    Hi Palov  As a first step, could you confirm please whether you are using Windows?  Thanks!

    0
    Comment actions Permalink
  • Palov

    HI MartyG,

    thanks for the reply! appreciate the help

    windows yes! AMD Radeon RX5700 XT +AMD Ryzen 7 3700 8-Core 3.59 GHz Windows 10 Home

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much.  If you are using Windows then the setup process for the Unity wrapper should be straightforward.

    1.  Install the full Windows version of the RealSense SDK using the installer file in the Assets file list on the SDK 'Releases' page.

    2.  Download the realsense.unitypackage file.

    3. Create a new Unity project with the '3D' template.

    4.  Double-leftclick on the realsense.unitypackage file whilst the new empty Unity project window is open.  This will import the RealSense files into the empty scene.

    5.  Go to the Assets > Scenes folder in Unity and double-leftclick on the StartHere scene file to load the RealSense starter scene, which is a list of buttons that launch RealSense tutorials.  It is the blue and white screen shown at the top of the Unity wrapper web page.

    6.  Make sure that the D435 camera is plugged in and then click the triangular Play button at the top of the Unity editor window to run the scene.  The program should then detect the camera and allow you to launch sample programs by left-clicking on the options.

     

    0
    Comment actions Permalink
  • Palov

    Thanks MartyG, That was very clear and worked perfect - thanks again!

    0
    Comment actions Permalink

Please sign in to leave a comment.