View my account

realsense D435/415 USB2.0 performance

Comments

1 comment

  • MartyX Grover

    Hi Djangotkscrivener  Information about the performance and supported configurations of RealSense 400 Series cameras on a USB 2 connection is provided in the link below.

    https://www.intelrealsense.com/usb2-support-for-intel-realsense-technology/

    Yes, you can stream depth and RGB simultaneously on a USB 2 connection at up to 30 FPS mode at 640x480 resolution.  Below is an image of a test that I ran with a D435i model in USB 2 mode with depth and RGB enabled at 640x480 and 30 FPS.  I ran multiple consecutive tests and performance remained consistent and smooth.

     

     

    And the image below is 1280x720 at 6 FPS:

     

    1
    Comment actions Permalink

Please sign in to leave a comment.