RealSense Support

Installed SDK and Viewer, but "Examples for Intel RealSense" is not working in Visual Studio.

Comments

1 comment

  • MartyX Grover

    Hi Arthurwuytens  If you are using Windows 10 then you can use an easy automated installer to install the Windows 10 version of the SDK.  It is located in an Assets file list at the bottom of the listing for each SDK version on the Releases page.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.42.0

     

     

    After downloading the file and running it to install the SDK, you can use Visual Studio props files provided in the SDK to create the linkages for Visual Studio projects that you have created.  There is a guide for doing so here:

    https://github.com/EduardoWang/visual-studio-real-sense-record-and-playback-project

     

     

    In regard to the existing SDK example programs, you can find pre-built executable versions of them by right-clicking on the RealSense Viewer launch icon that the SDK installer places on the desktop and selecting the Open file location menu option to open the SDK's Tools folder that contain tools and examples that can be launched with a double-leftclick.

    If an example program seems to launch but closes after a second, this likely means that it is one that needs to be launched from the Windows command prompt text interface rather than a double-leftclick from the Tools folder.

     

    If you would like to load the example programs into Visual Studio, the guidance in the link below will hopefully be of help:

    https://www.intel.com/content/www/us/en/support/articles/000030463/emerging-technologies/intel-realsense-technology.html

    1
    Comment actions Permalink

Please sign in to leave a comment.