RealSense Support

RealSense L515 USB 2.1

Comments

8 comments

  • Official comment
    Jesus Garcia

    Hello Sebastiancgonzalez,

    Your issue is being addressed via a private ticket therefore we will close this thread.

    Sincerely,
    Jesus G.
    Intel Customer Support

    Comment actions Permalink
  • Jdc

    I have the same issue as listed in the above post "RealSense L515 USB 2.1".  My L515 device initially recognized the USB3 and allowed me to change resolution settings RealSense Viewer, but subsequently only recognizes USB2.1 and the resolution is locked at 320 x 240.  I'm running Windows 10 on a Dell Precision 5750, and any suggestions/fix would be greatly appreciated... thanks  

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Jdc,

     

    Thank you for contacting us.

     

    Try flipping over the USB-C connector into the camera to insert it in the opposite polarity.

    In order to help us find the cause of these issues, can you tell us how the camera was used before the issue occurred? Was the camera dropped or banged against an object? 

    The answer to this question will not affect your warranty, but it will help us determine what is causing these issues.

     

    Regards,

    Zulkifli 

    Intel Customer Support 

    0
    Comment actions Permalink
  • Jdc

    I don't think it was dropped/banged, although the design of the box did cause a couple scares (the bottom slipping out and almost dropping).  I purchased an additional device to experiment w/ multi-camera capture/registration and, when setting up the second device, both began functioning @ USB3.2.  The behavior now seems somewhat unpredictable w/ the devices sometimes functioning at 2.1 at time and 3.2 at others.

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Jdc,

     

    Have you tried flipping over the USB-C connector into the camera to insert it in the opposite polarity? Some customers found success by doing it.

     

    In addition, please try on a different computer. Sometimes, the USB subsystem of a computer has an impact on how the camera is recognized.

     

    Regards,

    Zulkifli

    Intel Customer Support 

    0
    Comment actions Permalink
  • Adrian

    I have the same issue. I have tried all of the same fixes and none of them work. It was brand new out of the box and I had this issue. 

    0
    Comment actions Permalink
  • Alain

    I have the same issue. Brand new l515 out of the box. I am using realsense viewer on Windows 10 and the camera is recognized as USB 2.1 independently of the USB port it is connected to. Also, it only is recognized when the camera end of the cable is inserted in one way. Otherwise it is not recognized at all.

    Update. I opened the Depth.Quality.Tool, and to start with, the L515 was seen as USB3. But only for about half a minute, after that it switched to USB2.1  (as I was adjusting the camera position). And now the camera only appears as USB 2.1

     

    Any solution to this which seems to happen to quite a few people ?

    0
    Comment actions Permalink
  • Ydh

    나도 같은 문제가 있습니다.

    USB2.1 로만 연결이 되고, 3.0으로 연결되지 않습니다.

    2.1로 연결된 realsense viewer는 동작하지 않습니다. 카메라 화면이 전혀 보이지 않습니다.

    usb-c를 뒤집어 연결하면 아예 인식이 되지 않습니다. 2.1로만 연결되고, 연결되더라도 동작하지 않습니다..

    해결방법을 알려주세요..

    0
    Comment actions Permalink

Please sign in to leave a comment.