RealSense Support

L515 Range

Comments

1 comment

  • Aznie Syaarriehaah

    Hi Lucainnoc,

    The depth capture of L515 is starting from 0.25 to 9m and it performs best indoor with minimal exposure to the light.

    The maximum range of the L515 depends on laser power, receiver gain, object material, and ambient light. The camera can achieve it maximum possible range with a highly reflective object in a space with no ambient light. In your case, the performance is lesser might due to the presence of the ambient light and the poor reflection from the object. The L515 camera cannot be calibrated to improve performance. You have to adjust the setting base on your environment to get better performance of the camera.

     

    Check out the following article to have more detailed information regarding the L515 camera.

    Intel® RealSense™ LiDAR Camera L515 User Guide

    Regards,

    Aznie

    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.