RealSense Support

Factory calibration for D435i

Comments

1 comment

  • MartyG

    Hi Kota Mogami

    1.  If Dynamic Calibration is unable to be completed after multiple attempts, I would recommend one of the following options for technical support:

    a.  Post a help request on this forum.  Or;

    b.  If you have a Zendesk technical support account with Intel RealSense, contact Intel through that support channel.

    2.  Factory calibration involves calibrating both intrinsics and extrinsics.  The OEM Calibration Target system's OEM version of the Dynamic Calibrator software can also calibrate both (the normal version of the software only calibrates extrinsics).  So in that sense the factory calibration process and the OEM Calibration Target system are alike.

    In the majority of cases, the normal version of the Dynamic Calibrator software that only calibrates extrinsics should be sufficient to complete calibration successfully.

    3.  In cases where dynamic calibration repeatedly fails - perhaps due to a corruption in the camera's stored calibration table - then performing a Targetless calibration first and then following it up with a Targeted calibration may help.

    Performing a Gold Reset of the camera to its original factory calibration configuration with the Dynamic Calibrator software's CustomRW tool may also correct a damaged calibration table.

    1
    Comment actions Permalink

Please sign in to leave a comment.