RealSense Support

Has Infrared 1 1280x720 @ 6Hz Y8 been removed?

Comments

4 comments

  • MartyX Grover

    Hi Shibata664  1280x720 at 6 FPS is still available on D415 and D435 / D435i.  If you are using a D455 then 5 FPS is available at 1280x720.

    The UWP driver 6.1.160.21 is not required for using RealSense with Windows unless you need to interface with products that support the Microsoft Universal Windows Platform (UWP), such as the Hololens headset.  Most RealSense users do not need to have this driver installed. 

    If you do require UWP, I recommend using the earlier driver version 6.1.160.14 as the 6.1.160.21 driver has been reported to cause errors in some circumstances.

    https://downloadcenter.intel.com/download/28723/Intel-RealSense-D400-Series-Universal-Windows-Platform-UWP-Driver-for-Windows-10 

     

     

    0
    Comment actions Permalink
  • Shibata664

    Hi MartyG  I'm using the D415.  6.11.160.21 was recommended in the Recommended production camera configurations on this page, so I tried using it. 6.11.160.14 is no problem, right? 

    https://dev.intelrealsense.com/docs/firmware-releases

    rs-enumerate-devices.exe reports "Infrared 1 1280x720 @ 6Hz Y8" with the 6.1.160.14 driver. But the 6.1.160.21 driver doesn't report.  Is this change permanent?

    0
    Comment actions Permalink
  • MartyG

    You should not need to have the UWP driver installed in order to use this 6 FPS mode.  If your particular computer does insist on the driver's presence though then RealSense users who had problems with 6.1.160.21 (it should not affect available camera modes as far as I know) found that they did not have problems if the earlier 6.1.160.14 driver is installed.  

    0
    Comment actions Permalink
  • Shibata664

    I got it.

    0
    Comment actions Permalink

Please sign in to leave a comment.