RealSense Support

3d scanning human face

Comments

1 comment

  • MartyX Grover

    Hi Hdasilva1967  The point cloud will reflect the amount of the face that the camera was able to see.   If you have a single camera then you could take several scans of your head from the front, back, left and right and then stitch those individual clouds together into a single large 360 degree cloud.

    0.001 in the RealSense SDK is meters, not mm.  It is equal to a depth unit scale of 1 mm.

    0
    Comment actions Permalink

Please sign in to leave a comment.