RealSense Support

[WARN] .... : No RealSense devices were found!

Comments

25 comments

  • MartyG

    There was another case in which problems with the ROSBerryPi installation guide were mentioned.   I pointed them to the eleccelerator guide for installing librealsense, ROS  and the RealSense ROS wrapperon a Pi 4 with Raspian Buster.  This guide also links to the ROSBerryPi guide but has a list of suggestions for fixes for some of the errors that you may encounter during the ROSBerryPi guide's use.

    https://eleccelerator.com/wiki/index.php?title=Raspbian_Buster_ROS_RealSense 

    0
    Comment actions Permalink
  • A Dhesi2

    I have completed the instructions in this guide but when i try to run 

    roslaunch realsense2_camera rs_camera.launch

    the terminal window says "[WARN] [1599935053] No RealSense devices were found!"

    The eleccelerator guide does not mention this error.

    0
    Comment actions Permalink
  • MartyG

    Is the camera detectable by the rs-enumerate-devices tool please?

    0
    Comment actions Permalink
  • A Dhesi2

    yes and realsense-viewer

    0
    Comment actions Permalink
  • MartyG

    Do you get camera detection with roslaunch realsense2_camera rs_camera.launch

    If the above launch does work ... as the IMU topics are set to False by default from ROS wrapper 2.2.15 onward, I wonder if the open-source tracking launch file is looking for those D435i topics and cannot access them if you are using wrapper 2.2.15 or newer..

    0
    Comment actions Permalink
  • A Dhesi2

    How would I change the imu topics to true.

    when I run

    roslaunch realsense2_camera opensource_tracking.launch

    it says failed to meet update rate and no realsense devices were found. along with a few big red errors after a while saying rvis process has died, rtab process has died

    and when i run 

    roslaunch realsense2_camera rs_camera.launch

    it just says no realsense devices were found by itself

    0
    Comment actions Permalink
  • MartyG

    The IMU topics are set by enable_gyro and enable_accel

    I believe that the roslaunch terms to set both to true are:

    enable_gyro:=true enable_accel:=true

    0
    Comment actions Permalink
  • A Dhesi2

    i added enable_gyro:=true enable_accel:=true after 

    roslaunch realsense2_camera rs_camera.launch

    and

    roslaunch realsense2_camera opensource_tracking.launch

    and still got the same errors.

    I however noticed that when i run realsense-viewer it use librealsense 2.38.1 and realsense viewer detects the camera but when i use the other two above commands it uses librealsense 2.37.0 which doesn't detect the camera.

     

    0
    Comment actions Permalink
  • MartyG

    The recommended RealSense ROS wrapper version to match with SDK 2.38.1 is wrapper 2.2.17, which was released this week.

    https://github.com/IntelRealSense/realsense-ros/releases/tag/2.2.17 

    0
    Comment actions Permalink
  • A Dhesi2

    sorry i'm abit unsure on what i should do

    0
    Comment actions Permalink
  • MartyG

    In these situations, I believe that it is best to start again from the beginning and make sure that you have a rock solid stable librealsense installation on Pi 4 before seeking to add ROS.  The popular Acrobotic guide for setting up Pi 4 has a YouTube video version of their installation guidance.

    https://youtube.com/watch?v=LBIBUntnxp8 

    The original text version of their guide is here:

    https://github.com/IntelRealSense/librealsense/issues/7290#issuecomment-689615393 

    0
    Comment actions Permalink
  • A Dhesi2

    I've repeated all the steps again and am still receiving the same errors, I have tried to run

    roslaunch realsense2_camera opensource_tracking.launch
    roslaunch realsense2_camera rs_camera.launch
    0
    Comment actions Permalink
  • MartyG

    Ok, so you can confirm please that you have no problems at all with the camera in Librealsense with this new build based on the Acrobotic guide, and it is just ROS launch that has the camera detection problem?

    0
    Comment actions Permalink
  • A Dhesi2

    realsense-viewer works initially from using the acrobotic guide but after obtaining realsense2_camera from ROS, realsense-viewer no longer detects the camera and neither does

    roslaunch realsense2_camera rs_camera.launch

    , so i used this link:https://community.intel.com/t5/Items-with-no-label/RPi-4-Raspbian-Buster-realsense-viewer-cannot-detect-D435i/td-p/701349

    and this then made it so that realsense-viewer can once again detect the camera but

    roslaunch realsense2_camera rs_camera.launch

    still doesn't detect the camera. Therefore yes I can confirm this.

    0
    Comment actions Permalink
  • MartyG

    Of the two methods featured in the forum post that you linked to, did you use the libuvc-backend method please?  If so, that would make sense as it is a recommended means of installing librealsense on Raspberry Pi because it is suited to the Pi's Arm processor.

    https://github.com/IntelRealSense/librealsense/blob/master/doc/libuvc_installation.md 

    0
    Comment actions Permalink
  • A Dhesi2

    i did both methods

    0
    Comment actions Permalink
  • MartyG

    I see, that makes sense.  A problem with Pi 4 installations that can sometimes occur is an error that using -latomic fixes.  So from my previous experience of these cases, you should have a good and stable installation of librealsense set up on your Pi 4 after using -latomic.  So you just need to get it working with ROS now.

    0
    Comment actions Permalink
  • A Dhesi2

    Yes this is where i'm having problems, getting it to work with ROS, I keep getting errors saying it can't detect the camera still when running

    roslaunch realsense2_camera opensource_tracking.launch

    and

    roslaunch realsense2_camera rs_camera.launch
    0
    Comment actions Permalink
  • MartyG

    Ok, once you had installed librealsense using libuvc-backend and fixed the librealsense problems with -latomic, which method did you use to install ROS please?

    0
    Comment actions Permalink
  • A Dhesi2

    I followed the instructions on ROSberry for melodic (http://wiki.ros.org/ROSberryPi/Installing%20ROS%20Melodic%20on%20the%20Raspberry%20Pi) to install ROS then obtained realsense2_camera using section 4.2 of the above link. This then caused realsense-viewer to not detect the camera and when running

    roslaunch realsense2_camera opensource_tracking.launch

    the cameras wasn't detected aswell (same for this below command aswell)

    roslaunch realsense2_camera rs_camera.launch

    so then I obtained libuvc and added lbatomic thing to cmakelists.txt. This only sorted the problem out for realsense-viewer. and not for 

    roslaunch realsense2_camera opensource_tracking.launch

    roslaunch realsense2_camera rs_camera.launch

    0
    Comment actions Permalink
  • MartyG

    The usual order for setting up the ROS wrapper on librealsense is:

    1.  Install librealsense.

    2.  Install ROS (Kinetic or Melodic).

    3.  Install the RealSense ROS wrapper.

    *******

    As I understand it, using the ROSBerryPi guide installs ROS but does not install the RealSense ROS wrapper.  

    So once ROS has been successfully installed, it may be a good idea to try testing it to make sure that it is working before you move on to installing realsense2_camera.  A test command that you could try in the ROS terminal (getting the ROS version) is:

    rosversion roscpp

    0
    Comment actions Permalink
  • A Dhesi2

    when running rosversion roscpp i get 1.14.9

    0
    Comment actions Permalink
  • MartyG

    Okay, that sounds positive.  Hopefully we just need to install the RealSense ROS wrapper now (do not try to install librealsense once you have already set it up successfully in step 1 of this process).  This part - installing the RealSense ROS wrapper - seems to be the point where things are most likely to go wrong.

    I am hesitant to suggest using the official instructions on the RealSense ROS wrapper as they are primarily aimed at Ubuntu installation rather than Raspbian Buster.  The eleccelerator guide may therefore be the most suitable one, as it is designed specifically for Raspbian Buster and Pi 4.  

    https://eleccelerator.com/wiki/index.php?title=Raspbian_Buster_ROS_RealSense#Installing_ROS_Package:_realsense-ros 

    BUT I am aware that you have already tried this guide earlier and got the same error when using roslaunch.

    Looking at their method, it seems most likely to work if librealsense SDK version 2.38.1 was installed in step 1.  This is because it installs the newest version of the RealSense ROS wrapper by cloning the RealSense ROS GitHub. 

    Can you confirm that you have librealsense SDK 2.38.1 currently installed, please?

    If you do use the eleccelerator guide again to try to install realsense2_camera, please do not go further down past the end of the Installing ROS Package: realsense-ros section as we do not currently want to install RTABMAP.

    Thank you very much for your patience so far.

    0
    Comment actions Permalink
  • A Dhesi2

    Thank you Marty I'm very grateful for this help. Where I was going wrong was not obtaining the ROS wrapper properly, I have it now and have completed the three steps:

    1.  Install librealsense. (using acrobotic guide)

    2.  Install ROS (Kinetic or Melodic).

    3.  Install the RealSense ROS wrapper.

    I have librealsense SDK 2.38.1 installed.

    When i got realsense2_camera from ros it also gave me librealsense sdk 2.37 aswell however, This is because on https://github.com/IntelRealSense/realsense-ros/ it says

    "This will install both realsense2_camera and its dependents, including librealsense2 library.

    Notice:

    • The version of librealsense2 is almost always behind the one availeable in RealSense™ official repository."

    I'm assuming i would now get RTAB-MAP

    0
    Comment actions Permalink
  • MartyG

    There are two official ROS wrapper installation methods, Method 1 and Method 2, and you use one or the other.  The first method is easier as it installs librealsense and the ROS wrapper together.  Like the message said though, because it is installing from packages the installed librealsense version may be a bit older than the newest one that Method 2 installs (e.g 2.37.0 instead of 2.38.1).  

    Everything seems to have worked out for you now though and you have a template to follow if you have to repeat it in future.  So that is great news.

    Yes, the next logical step will be RTABMAP_ROS if you are using the D435i SLAM guide.

    0
    Comment actions Permalink

Please sign in to leave a comment.